You are here: Getting Started > Testing and Debugging the Project > Variable Animation

Variable Animation

When your application is running, all variables in the IEC 61131-3 Editors, in the Dictionary and in the Watch Window are animated. This means that the value of each variable is displayed dynamically.

About Online Change

When Online Change is enabled,the animated values only take place when you are in Debug mode (and not edit).

Limitations

 

Variable Monitoring

IEC 61131 Editor Debugging


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™